Evolución de la red de programadores
Migrating to IP Distribution over CDN
CommScope's DigiCipher Streaming solution offers a low-risk migration path that leverages existing integrated receiver decoders (IRDs) from satellite to Internet protocol (IP) content distribution network (CDN) input, which creates new distribution efficiencies and prevents service interruption. Through this cutting-edge system, programmers can lower their satellite dependency while keeping command and control over video distribution without compromising reliability or security.
Best of all, programmers can add more IP distribution sites incrementally on demand without needing an entirely new secondary system.
Desafíos y oportunidades
![DigiCipher-Streaming-PP1-hero500](/globalassets/digizuite/944360-digicipher-streaming-pp1-hero500.jpg?w=400&h=203&mode=crop)
Low-risk migration
CommScope's DigiCipher Streaming solution allows programmers to utilize existing resources and architecture in their satellite distribution operations to achieve IP CDN delivery. By using our next generation integrated receiver decoders (IRDs), programmers can deliver video inputs over both radio frequency (RF) and IP allowing video distributor packager (VDP) to use the same equipment regardless of satellite or terrestrial delivery.
![DigiCipher-Streaming-PP2-hero500](/globalassets/digizuite/944364-digicipher-streaming-pp2-hero500.jpg?w=400&h=203&mode=crop)
Time-tested encryption
Programmers can use content that's already encrypted for satellite distribution and simply package it for IP distribution. No re-encryption necessary. So, they can deliver content over IP CDN methods using the exact same industry-tested and uncompromised DigiCipher-II encryption they've come to know and trust.
![DigiCipher-Streaming-PP3-hero500](/globalassets/digizuite/944361-digicipher-streaming-pp3-hero500.jpg?w=400&h=203&mode=crop)
Complement satellite distribution
With the new VDP-1000 packager, programmers can look to terrestrial-based CDN solutions for content distribution. This can aid multichannel video programming distributor (MVPD) affiliates in moving to all IP operations.
![DigiCipher-Streaming-PP4-hero500](/globalassets/digizuite/944367-digicipher-streaming-pp4-hero500.jpg?w=400&h=203&mode=crop)
Centralized distribution
Through DigiCipher Streaming, programmers can also remove concerns around satellite footprint constraints by centralizing worldwide distribution. Plus, content replacement and time-shift applications are possible, which can unlock future cost efficiencies and open up new revenue opportunities.
![DigiCipher-Streaming-PP5-hero500](/globalassets/digizuite/944362-digicipher-streaming-pp5-hero500.jpg?w=400&h=203&mode=crop)
Uninterrupted service
By leveraging existing IRDs in the migration from satellite to CDN IP input, programmers can avoid service interruption. Additionally, the CommScope DigiCipher Streaming redundant CDN design allows for uninterrupted service in the event of major primary CDN outages.
¿Por qué CommScope?
Video content delivery innovation
CommScope has been in the forefront of video content delivery by providing cutting-edge content distribution solutions to Programmers and Video Providers for more than 35 years. Our cutting-edge solutions include a portfolio of robust and feature-rich products that offer deterministic performance and reliability.
El presente se encuentra con el futuro
CommScope continues to shape the networks of the future. Our extensive portfolio, flexible architecture and professional services capabilities enable programmers and video providers to continually evolve their distribution networks. Siempre estamos anticipándonos al futuro, para garantizar que siempre esté un paso adelante.
Fiabilidad sin precedentes
La satisfacción del suscriptor depende de la fiabilidad de su infraestructura física. Descubra cómo nuestras soluciones pueden ayudar a que sus redes “siempre conectadas” sigan en funcionamiento.
Recursos destacados
Cambie de satélite a CDN
Infografía
Tiempo para que las redes de distribución del programa regresen a la normalidad.
ViacomCBS se asocia con CommScope para liderar la migración de distribución de contenido industrial de satélite a IP de CDN
Nota de prensa
Los canales lineales DABL, FAVE y SHOWTIME seleccionados utilizan las soluciones de video CommScope IP para la entrega de contenido como parte de la transformación digital a gran escala de ViacomCBS.
![500 x 281 home-network-bandwidth-streaming-hero Card Hero](/globalassets/digizuite/919092-home-network-bandwidth-streaming-hero.png)